Funding of European solar startups up almost 400%
Total investment in European solar startups is up 398% on last year, with firms receiving $6 billion in backing by the end of May 2023 compared with $1.2 billion raised by the same point in 2022. Globally, investment in the category is up 47%, with funding of the sector down 7% in the US so far this year, reveals new research by Avnet Abacus, an electronics distributor that consults engineers when they’re designing new products.

Avnet Abacus analysed Crunchbase data for companies listed under solar and other renewable energy categories to provide insight on the level of funding going into these areas.
Commenting on the study’s findings, Dr Sara Ghaemi, Avnet Abacus’s Technical Director, says “Even though solar technology is relatively mature, there is still a lot of room for growth and innovation. There is growing demand around the world, and government policies and incentives continue to support investment in this area, with engineers continually seeking new ways to make solar more efficient.”
European solar startups raise $6 billion in just 5 months
By the end of last year, Europe’s solar startups had drawn in $7.2 billion in funding, almost four times higher than the previous year’s record of $1.9 billion. So far in 2023, Europe’s solar ventures have already raised $6 billion, 83% of last year’s total, before even reaching the midway point in the year.

Investment in startups in the broader renewables category is up 27% worldwide compared to this time last year, but with a 25% ($4 billion) drop in Europe. And VC funding across all European startups, in any sector, decreased 66% year-on-year in Q1 of this year.
Average funding round for European solar startups at record high of $166.1 million
Despite the continued uncertainty in the venture capital market, average investment in European solar is at an all time high at $166.1m, compared with an average of $88.3m in 2022 and $22.9m in 2021. The mean amount of venture capital flowing into European solar so far this year ($166.1m) eclipses the category’s global average of $116.8m and US average of $113.8m.

Rooftop panels lead the expansion, but large scale solar required to replace fossil fuels
Although wind produces double the amount of the EU’s electricity as solar, generating 15.9% compared with solar’s 7.6%, there are almost 6 times more startups focused on solar than wind energy in Europe, and it’s the consumer market that’s driving the expansion.
Rooftop installations account for 66% of the EU’s current solar capacity, with commercial roof-top panels spreading faster than utility-scale ground-mounted projects. And consumers keen to curb rising electricity prices are also looking to the sun, with Google searches about the cost of solar panels hitting an all-time high last summer with search interest up over 300% compared with the previous year.
Dr Sara Ghaemi, Avnet Abacus’s Technical Director, comments “Rooftop solar panels could potentially produce 25% of Europe’s annual electricity consumption. As well as the available rooftop surfaces, the facade of the buildings can also contribute to the generation of green energy. The fast deployment and decentralised integration of photovoltaic panels into the energy system are two main attributes that make them very attractive.”
“When looking for a replacement to fossil fuels, however, rooftop and facade panels will not be enough. This will require large scale photovoltaic farms, where you’re talking about megawatts of power generation. At such high power and high energy density, recent developments in silicon carbide and gallium nitride technologies are enabling power to be converted with greater efficiency than traditional silicon-based components.”
Discover how Avnet Abacus and our trusted suppliers can transform your smart energy solutions. Contact us today to unlock the power of sustainable innovation.
Contact Us