Smart Healthcare

Extend your healthcare offering by embracing connectivity

AVA - IoT - Healthcare - Sub Navigation

Display portlet menu

Giving medical professionals the most advanced tools to deliver better healthcare

IoT introduces a new paradigm to patient-centric healthcare. Avnet can help you do more, from capturing patient-generated health data to monitoring chronic health conditions. Use IoT technologies to add remote patient monitoring and deliver more informed care.

doctor reviewing scans

Learn more - Intro Static HTML_1

Display portlet menu

Learn More

 

Applications

There are many potential use cases for IoMT. They range from monitoring vital signs such as heart rate and blood pressure using wearables to the intelligent hospital room that monitors both patients and tracks the movements of medical staff and automates the delivery of supplies. According to Avnet Abacus, the most important applications are telehealth, advanced diagnostics, and robotic surgery.

Telehealth

With the help of IoMT devices, vital parameters can be continuously monitored remotely. This allows for quick detection of anomalies, and medical professionals can be promptly alerted. This not only ensures timely intervention but also reduces the number of hospital admissions. Intelligent and wearable solutions for monitoring blood sugar levels, connected inhalers for controlling and predicting asthma attacks, or ingestible sensors for gathering information from the digestive system are just a few examples of IoMT devices. For many diagnoses, a visit to a doctor's office is no longer necessary – with the appropriate connected devices, diagnoses can be made remotely, allowing healthcare to take place in the patient's home.
 

Advanced diagnostics

The continuous collection of vital parameters through IoMT devices, combined with advanced data analysis, significantly improves medical diagnostics. With the help of AI and ML algorithms, large amounts of patient data can be processed – enabling faster and more accurate diagnoses.
 

Robotic surgery

The integration of IoMT technology allows surgical robotic systems to connect with external devices and doctors. IoMT-enabled robotic systems have already been used in many applications, including microsurgery and minimally invasive surgery. Surgeons can connect with telesurgery centres via IoMT and even operate surgical robots remotely without being physically present. Since 2019, remote surgical procedures have been performed worldwide, notably in China. For example, a medical team from Beijing performed eye surgeries from a distance of 3,000 km
 

Technological challenges

Although the potential of IoMT is immense, there are also challenges to consider. Data security and privacy are of utmost importance. Ensuring secure data transmission and storage is crucial for protecting patient information. Additionally, the development of industry-wide standards that enable data exchange and interoperability between devices is essential for the widespread adoption of IoMT and the realisation of its full potential. To make medical decisions based on IoMT data, the collected information must meet the highest standards of accuracy and reliability, and the IoMT devices must comply with international certifications for medical devices. Wearables must function reliably over a long period while being as lightweight and small as possible to ensure comfortable wear, which poses particularly high demands on the devices' power supply , among other aspects.
 

IoMT devices

The devices that collectively form the IoMT can be classified into many different categories. Large, stationary devices such as MRI systems are included, as well as infusion pumps, blood glucose meters, smart thermometers, and heart rate monitors. Personal emergency response systems and remote patient monitoring devices make up a large part of the IoMT product list. A growing segment of the IoMT consists of tiny ingestible sensors and cameras that perform medical tasks such as endoscopies. At the forefront, however, are undoubtedly wearables: they range from fitness trackers and smartwatches to more specialised medical wearables such as heart rate sensors. These devices must be designed to be user-friendly, unobtrusive, and connected, enabling the continuous collection of health data in real time.
 

Device selection

When selecting devices for the Internet of Medical Things, several factors must be considered. These include compatibility with existing healthcare infrastructure, the accuracy of data collection, and, particularly for wearables, comfort and secure long-term power supply. Additionally, the aspect of continuous updating and maintenance should not be overlooked to ensure that the devices function optimally and provide reliable data for medical personnel.
 

How technology is enabling smart healthcare

Patient monitoring

Smart sensors and wearable technologies can provide valuable information about patient activity, location and physical condition. Patient data is securely shared through the cloud to enable care professionals to make informed decisions.


Gain more insights

Analyze patient-generated health data using AI and machine learning, to give care providers and practitioners a rapid assessment of patient health.


Provide care remotely

IoT technologies offer the ability to administer care remotely. Patients can consult with doctors from their own homes, reducing the need to travel and giving patients with chronic conditions a more personalized in-home experience.


Care where it is needed

Many conditions need regular assessment. IoT provides that always-on experience while relieving care providers from the intensity of home visits and long travel times.

AVA - IoT Healthcare - Suppliers - Static HTML

Display portlet menu

Featured Suppliers

 

 

 

 

 

Related Articles

Learn how AI and the latest CPM technologies optimize patient rehabilitation - Webinar - Grid Box Light

Display portlet menu

Webinar

AI and the latest CPM technologies optimize patient rehabilitation

Continuous passive motion (CPM) is now a critical part of patient rehabilitation. New technologies, including artificial intelligence, are helping medical OEMs take the next step to optimize patient therapy.

learn-how-AI-and-the-latest-CPM-technologies-optimize-patient-rehabilitation

Display portlet menu

Using sound to capture medical data boosts device innovation - Webinar - Grid Box Light

Display portlet menu

Webinar

Using sound to capture medical data boosts device innovation

Wearable medical devices provide continuous body monitoring. Acoustic sensing is non-intrusive and the data supports early diagnosis and remote analysis. Are the stethoscope’s days numbered? That’s not likely, but new device opportunities abound.

Designers lead advances in CT scanning field - Webinar - Grid Box Light

Display portlet menu

Webinar

Designers lead advances in CT scanning field

Computed tomography is an advanced medical imaging technology. New developments are making it even more useful for healthcare professionals and safer for patients.

Safer targeted approaches to treat atrial fibrillation - Webinar - Grid Box Light

Display portlet menu

Webinar

Safer, targeted approaches to treat atrial fibrillation

Pulsed field ablation is a bold approach to treating atrial fibrillation. The control required is extreme, leading to innovative solutions and newly patented technologies gaining attention from doctors, patients and OEMs.