TDK

TDK Corporation is one of the world's leading manufacturers of electronic components and systems. TDK's portfolio includes passive components, such as ceramic, aluminum electrolytic and film capacitors, ferrites and inductors, high-frequency products, and piezo and protection components, as well as sensors and sensor systems. These products are marketed under the product brands TDK, EPCOS, InvenSense, Micronas, and Tronics. TDK focuses on demanding markets in the areas of information and communication technology and automotive, industrial and consumer electronics. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America.

TDK focuses on demanding markets in the areas of information and communication technology and consumer, automotive and industrial electronics. The company has design and manufacturing locations in Asia, Europe, and in North and South America.
Official logo of TDK
ZUBoard 1CG Development Board

ZUBoard 1CG Development Board

The ZUBoard 1CG provides ample flexibility and versatility to experiment with and learn the AMD-Xilinx Zynq®️ UltraScale+™ architecture. This affordable device features 81K programmable logic cells with a Dual-core Arm®️ Cortex®️-A53 MPCore™.

RASynBoard Evaluation Kit

The RASynBoard eval kit is based on the RASynBoard module, a tiny (25mm x 30mm), ultra-low power, edge AI/ML board, based on a Syntiant NDP120 Neural Decision Processor, a Renesas RA6M4 host MCU plus a powerefficient DA16600 Wi-Fi/BT combo module.

TDK-Lambda

For more information about Lambda (TDK) and their product offerings