2404-how-ai-trism-is-laying-foundations-of-trust

Display portlet menu

2404-how-ai-trism-is-laying-foundations-of-trust

Display portlet menu

How AI TRiSM is laying foundations of trust for the Future of AI

Conceptual image of smart car in purple

The rapid development of the large generative AI model ChatGPT has recently been in the spotlight, both for its limitless potential and the grave risks it poses. While generative AI has the ability to transform the way businesses work and compete, it also presents new risks that traditional controls are powerless to address. In particular, the risks associated with hosting cloud-based generated AI applications are serious. And, they are multiplying at an alarming rate.

Againt this backdrop, a new term has emerged – AI TRiSM.

AI TRiSM stands for “Artificial Intelligence (AI) Trust, Risk and Security Management”. An AI governance framework proposed by Gartner in 2022, it aims to assure enterprises that AI models are safe, trustworthy, effective and fair. In this era of flourishing AI, data communications and GPUs, the AI TRiSM framework is becoming increasingly important.

AI’s “Auditor”: Helping AI Do Good

As AI technology continues to rapidly evolve, we are seeing various large-scale AI models vying for the top spot, from the hundreds at a domestic level to the thousands around the world. As these AI models become increasingly complex and their parameters multiply exponentially, it becomes increasingly critical to ensure their transparency, fairness and reliability. Especially when enterprises integrate third-party AI models and tools, they must consider the risks involved in the large data sets on which these models rely. In addition, users may be exposed to sensitive data in other AI models, which could have serious regulatory, business and reputational consequences for the organization.

How AI TRiSM is laying foundations of trust for the Future of AI

As a comprehensive management framework that helps identify and mitigate potential risks such as bias, misunderstanding, and abuse lurking in AI applications, AI TRiSM plays an essential role in this auditing process. In the field of image recognition, for instance, AI TRiSM can help enterprises identify and eliminate bias in models to guarantee fairness to all users. In the field of natural language processing, AI TRiSM can help prevent models from being abused or used to generate false information. Similarly, in the field of machine learning, AI TRiSM can ensure model reliability and validity. For example, when it comes to medical diagnoses, it can evaluate the accuracy of the machine learning model.

AI TRiSM is not only about managing risk, but also about the ability to use AI responsibly and ethically. It involves a comprehensive set of tools to preemptively identify and mitigate risks posed by AI, ensuring compliance with transparency, security and privacy standards.

The “Guardian” of Data Communications: Building a Strong Network Security Barrier

Data communications are at the core of modern information technology. With the development of 5G and IoT, the speed and complexity of data transmission are increasing at an unprecedented rate. As more and more devices and services rely on IoT, AI TRiSM leverages encryption technology, network monitoring and timely security response mechanisms to ensure data safety during transmission. This involves not only the safeguarding of consumer data, but also the protection of national security and critical infrastructure.

How AI TRiSM is laying foundations of trust for the Future of AI

AI TRiSM provides the necessary tools and framework to ensure risks are identified and managed during data transfer. It therefore helps determine potential security vulnerabilities and guarantees the security and privacy of data during transmission.

The “Defender” of GPUs: Helping Them Reach Their Maximum Potential

The core hardware of AI and deep learning, graphics processing units (GPUs) are critical to AI systems, especially when dealing with massive amounts of data and complex algorithms. As GPUs develop in leaps and bounds, AI TRiSM will play an increasingly important role in safeguarding their performance and security.

AI TRiSM measures for GPUs include optimizing processor performance, monitoring and preventing potential hardware failures, and ensuring safety during data processing. As AI models become more intricate and data-intensive, securing the efficient and stable operation of GPUs will be key to accelerating the deployment and promotion of AI applications.

AI TRiSM’s role in the GPU field primarily centers on ensuring the safety of the computing process and optimizing the use of GPU resources. In autonomous vehicles, for instance, AI TRiSM ensures that the data processed by the GPU is not affected by external attacks while fine-tuning algorithms to improve processing efficiency. AI TRiSM complies with standards such as ISO 26262 and ISO 21434, thereby meeting the highest levels of functional safety and automotive cybersecurity practices, respectively.

Conclusion

The application of AI TRiSM in the fields of AI, data communications and GPUs is key to maintaining balance and security in the rapidly evolving world of technology. Implementing and enforcing AI TRiSM in these areas will not only improve the performance and reliability of AI systems, but also protect user data and maintain network security. The healthy development of AI technology depends on it.

According to Gartner’s analysis, AI models that deliver AI transparency, trust and security will achieve a 50% rise in adoption rates, business goals, and user acceptance by 2026.

In the future, AI TRiSM will undoubtedly continue to play an integral role in safeguarding users from the emerging and terrifying new risks posed by the unstoppable rise of AI . Already, it is laying the foundations for building a smarter, safer and more reliable digital world.

 

2404-how-ai-trism-is-laying-foundations-of-trust

Display portlet menu

2404-how-ai-trism-is-laying-foundations-of-trust

Display portlet menu
Related Articles
Integration of Multiple Technologies Heralds a New Era in Smart Healthcare
The future of AI is at the edge
May 10, 2025
As AI technology gains traction and the concept of green computing is embraced, edge devices will become an increasingly powerful force driving the development of a more intelligent world.
Integration of Multiple Technologies Heralds a New Era in Smart Healthcare
The invisible force improving the way we work and live
April 15, 2025
Having foreseen the growth potential of ambient invisible intelligence, Avnet provides a full range of innovative products and solutions to meet evolving market needs in this dynamically expanding field.

2404-how-ai-trism-is-laying-foundations-of-trust

Display portlet menu
Related Events
Avnet/ Renesas AI webinar
Date: July 15, 2020
Location: Webinar