Franchised Partner

AMD

AMD develops highly flexible and adaptive processing platforms that enable rapid innovation across a variety of technologies – from the endpoint to the edge to the cloud. AMD is the inventor of the FPGA, hardware programmable SoCs and the ACAP, designed to deliver the most dynamic processor technology in the industry and enable the adaptable, intelligent and connected world of the future. For more information, visit www.amd.com.

Manufacturers Categories Static HTML

Display portlet menu

EBV - Product Highlights - AMD Smart Door Lock (GBL)

Display portlet menu

AMD Smart Door Lock

Step into the future of home security with smart door locks, where cutting-edge technology meets convenience. One standout innovation in door locks is the integration of camera-based AI systems for face-recognition.

EBV - Motor Control - Product Highlights (GBL)

Display portlet menu

Motor Control Solutions

Digital motor control can be defined as a drive system that combines an electric motor with power electronics for its energy delivery and processor units for motion control, as well as sensor and communication interfaces.

EBV - Product Highlights - AMD KRIA Adaptive MC SOMs (GBL)

Display portlet menu

AMD Kria™ Adaptive Motor Control SOMs

AMD is focused on developing power-efficient and highly deterministic industrial solutions suitable for large-scale deployments. The AMD Kria™ starter kit offer a latency advantage when compared to competitive products.

EBV - AMD-Xilinx - Kria SOM Family Highlights (GBL)

Display portlet menu

AMD Kria™ SOM Family

AMD Kria™ SOM Family is ideal for Edge and Vision Application Development and features a custom custom-built Zynq™ UltraScale+™ MPSoC device in a small form factor card.

EBV - Product Hightlights - AMD Healthcare (GBL)

Display portlet menu

Adaptive & Intelligent Healthcare Solutions from AMD

Technological advancements that are creating solutions for earlier detection, better imaging, and virtual and robotic-assisted care have the ability to help healthcare providers increase patient outcomes and provide more effective personalized care.

EBV - AMD - ZUBoard 1CG Highlights (GBL)

Display portlet menu

AMD ZUBoard 1CG

The ZUBoard 1CG provides the flexibility and versatility for engineers to experiment with and learn the AMD Zynq™ UltraScale+™ architecture.

EBV - Product Highlights - AMD Xilinx Industrial Robotics (GBL)

Display portlet menu

AMD Industrial Robotics

Discover how the AMD Kria™ robotics starter kit, along with the Kria™ robotics stack, enables rapid development for robotics, machine vision, and industrial communication and control, through adaptive computing.

EBV - AMD robotics starter kit (GBL)

Display portlet menu

AMD Kria™ KR260 Robotics Starter Kit

The AMD Kria™ KR260 Robotics Starter Kit integrates high-performance industrial interfaces and features native ROS 2 support. It enables roboticists and industrial developers without FPGA expertise to develop hardware accelerated applications.

Xilinx Featured product highlights (LC)

Display portlet menu

Featured product highlights

EBV - AMD Automotive Highlights Grid Box Light (GBL)

Display portlet menu

Driving Automotive Innovation with AMD

From automation to electrification to infotainment and beyond, we’re helping our customers like you deliver the next generation of cutting edge automotive designs.

EBV - MiniZed Dev Board Grid Box Light (GBL)

Display portlet menu

AMD MiniZed Development Board

Featuring a AMD Zynq™ Z7007S, which integrates an Arm Cortex-A9 processor with AMD Artix™ 7 programmable logic, the MiniZed is a low-cost yet versatile development board targeted for entry-level Zynq designs.

EBV - Xilinx - U250 Alveo Grid Box Light (GBL)

Display portlet menu

U250 Alveo™ Data Center Accelerator Cards

Learn about Xilinx® U250 Alveo™ Data Center accelerator cards, designed to meet the constantly changing needs of the modern Data Center.

EBV - AMD - Hackster Grid Box Light (GBL)

Display portlet menu

Hackster.io AMD Projects

Everything you need to get going fast!

EBV Xilinx NPI teaser (NPI-table)

Display portlet menu
Image Product Description Link New

EBV - AMD - Related events Static HTML

Display portlet menu

 

Related events

Xilinx - Getting Started with the Ultra96-V2 Development Board - Grid Box Light - Simple

Display portlet menu

Image of Xilinx Ultra96 V2 board

Webinar: Getting Started with the Ultra96-V2 Development Board

Available on demand

This training is held by Mario Bergeron. Mario is a Technical Marketing Engineer for Avnet, specialized in embedded vision and machine learning. After his degree in Computer Engineering (B.Sc.) from Université Laval in Québec City, he started his career as an ASIC designer, and has since then accumulated over 25 years of DSP and FPGA based embedded design experience. Present activities include deep learning platforms, reference designs, and customer training.

Register Now

EBV - Xilinx - Accelerating AI Camera Development Grid Box Light (GBL)

Display portlet menu

Accelerating AI Camera Development with AMD Vitis™ Software Platform

Check out the On-Demand webinar from AMD. During this webinar we will explore this topic from a variety of different perspectives.

Xilinx: Cost-Optimized Portfolio for Industrial Cameras | EBV Elektronik

Display portlet menu

AMD: Cost-Optimized Portfolio for Industrial Cameras

Online, On demand

This presentation explores some of the trends driving new processor requirements in industrial cameras and provides examples of Xilinx's recent solutions that offer increased performance per watt and unlock intelligence, resolution, and speed for compact form factor cameras

EBV Xilinx NPI headline (html)

Display portlet menu