{}
About Author

-
More From Author

An introduction to EV charger design: the power stages
Semiconductors are key to efficiency, low cost, small size and ultimately commercial success of electric vehicle DC chargers. In this blog we consider some of the trends, options and their tradeoffs.

Mehr Effizienz Im Gesundheitswesen
Daher wandert auch hier immer mehr intelligenz in die fläche; wearables können heute vitaldaten nicht nur erfassen, sondern auch analysieren. Intelligente assistenten unterstützen die mitarbeiter an den unterschiedlichsten stationen.

Greater Efficiency in Healthcare
Intelligence is increasingly migrating to the edge: not only can wearables today record vital data, they can also analyse this information instantly. Smart assistants support employees in healthcare in an incredible variety of ways.

Lernende Roboter Passen Sich An Ihre Aufgaben Und Umgebung An
Zukünftig können die mechanischen helfer ohne programmierung unterschiedliche objekte greifen und sich in komplexen umgebungen unabhängig bewegen.

How Learning Robots are Adapting to Their Tasks and Environment
While robots required complicated programming by experts in the past, the systems will be able to teach themselves how to carry out their tasks in the future. This will allow robots to adapt autonomously to changing surrounding circumstances

Von Der Vorausschauenden Wartung Bis Zum Kollaborativen Roboter
Die KI kann zum Wachstumsmotor für die Industrie werden: Alleine in Deutschland könnte bis 2030 das Bruttoinlandsprodukt durch den frühen und konsequenten um bis zu vier Prozent höher liegen als ohne den Einsatz von KI

From Predictive Maintenance to Collaborative Robots
AI and machine learning are exploiting opportunities in connection with Industry 4.0 in particular because enabling a production operation to organize itself autonomously and respond flexibly takes huge volumes of data.

Smart Cameras Keep Everything Squarely in Their Sights
Smart cameras can process imagery autonomously before initiating responses of their own accord. In industrial applications, they are used for quality control or to control plants and systems.

FPGA vs. GPU vs. CPU – hardware options for AI applications
Field programmable gate arrays (FPGAs) deliver many advantages to artificial intelligence (AI) applications. How do graphics processing units (GPUs) and traditional central processing units (CPUs) compare?

Top 10 pitfalls in developing machine vision systems with artificial intelligence
Machine vision (MV) and artificial intelligence (AI) provide valuable inspection and analysis capabilities to a wide range of leading-edge applications. As with all advanced technologies, there are pitfalls to avoid.

IoT Platforms: Build, Buy, or Both?
With the accessibility, affordability and overall democratization of technology, it is tempting today to try and do everything yourself.

Don't reinvent the wheel when it comes to IoT
EBV’s scalable, repeatable vertical SaaS applications are each between 60 and 80% complete, speeding time to market in IoT.

Designing for the IoT as Intelligence Moves to the Edge
The Internet of Everything will be all inclusive, from huge data centers to single-purpose sensors. While individual power requirements vary across the IoT, the need for energy efficiency will be present everywhere.

Building the right security foundation for connected devices
Advances in IoT have led to a boom in connected devices, so security is more important than ever. Discover how to build the right security foundation.

The State of Automotive Only Starts with Autonomous Driving
Learn how the state of automotive spans a variety of applications, from electrication to in-cabin AI.

Somewhere Between the Flintstones and the Jetsons
Learn more about developing adaptable automotive automation with Xilinx

Redefining nanopower for the Internet of Things
Internet of Things trends today revolve around shiny objects—whether they be artificial intelligence or blockchain—but what if one of the most revolutionary parts of the IoT is something designers consider every day in devices?

Is best in class the only consideration for your analog design?
It’s easy to seek out the absolute top of the line when it comes to a design. Whatever the “best” part is, is probably what’s going to be the most compelling for your design, right?

Designing Reliable Analog Circuits in a Less-Than-Reliable World
Analog touches everything. If not for the multitude of analog and mixed-signal components that vendors have developed in the past decades, the digital “revolution” that has made so many industry sectors leap forward would not be possible.

Connectivity Among Major Analog Design Considerations in Health Wearables
Development of very low powered analog body sensors, digital microcontrollers, and innovative power and battery management circuits are driving the growth of wearable healthcare products.

6 Unique Op Amp Circuits
Electronics circuits evolved from discrete circuits to highly integrated circuits (IC) on a single chip enabling highly advanced analog and digital systems saving space and cost. An operational amplifier (Op Amp) is one such integrated circuit that has pl...

KI-Pionier Minsky: Vorläufig tot?
Das Gehirn funktioniert wie eine Maschine, so die These von einem der wichtigsten Pioniere der Künstlichen Intelligenz. Also kann man es nachbauen – und sich durch ein Back-up des Bewusstseins auf einem Rechner unsterblich machen.

AI-pioneer Minsky: Temporarily dead?
The brain functions like a machine, or so according to the theory of Marvin Minsky, one of the most important pioneers of artificial intelligence. In other words, it can be recreated – made immortal by backing up its consciousness onto a computer.

Neuronale netze simulieren das gehirn
Mit verschiedenen Ansätzen der Datenauswertung sollen Maschinen intelligent werden. Im Fokus steht dabei nicht nur die Leistungsfähigkeit, sondern immer mehr auch eine Flexibilität, wie sie das menschliche Gehirn bietet.

Ist KI besser als der arzt?
Kognitive Computerassistenten helfen Medizinern bei Diagnose- und Therapieentscheidungen. Sie sind deutlich schneller bei der Auswertung von medizinischen Informationen und erreichen mindestens die gleiche Präzision.

AI better than the doctor?
Cognitive computer assistants are helping clinicians to make diagnostic and therapeutic decisions. They evaluate medical data much faster, while delivering at least the same level of precision.

Neuronal networks simulating the brain
Machines are being made more intelligent based on a variety of data analysis methods. The focus of these efforts is shifting increasingly from mere performance capability towards creating the kind of flexibility that the human brain achieves.

Ist Teleportation möglich?
In den Star-Trek-Filmen werden Menschen einfach per Knopfdruck von einem Ort zum anderen gebeamt. Was nach reiner Science Fiction klingt, ist dank der Quantenphysik heute tatsächlich schon Realität.

AI Smarter than humans?
What began in the 1950s with a conference has grown into a key technology. It is already influencing our lives today, and as the intelligence of machines increases in the future that influence is bound to spread much more.

In eine kabellose Zukunft dank drahtloser Kommunikation
Das Internet der Dinge wird zunehmend zur Realität, immer mehr Maschinen, Geräte, Gegenstände und letztlich auch Menschen vernetzen sich.

Is teleportation possible?
In Star Trek, people are simply beamed from one place to another at the push of a button. What sounds like pure science fiction is actually already reality today thanks to quantum physics …

Smart City Projekte und Technologien
Smart Cities leben von einer Vielzahl an Informationen, die von Menschen, Geräten und Sensoren übertragen werden.

Höhere Vernetzung, Geringerer Stromverbrauch
Mit der explodierenden Zahl an vernetzten Geräten und dem rasant steigenden Datenvolumen rückt die Energieeffizienz der Wireless-Technologie zunehmend in den Fokus.

Smart networks for smarter cities
Smart cities subsist on a large amount of information which is transmitted by people, devices and sensors. A wide range of wireless technologies is used for this purpose, depending on the application in question.

Higher networking, lower power consumption
Due to the explosion in the number of networked devices and the rapidly increasing data volumes, energy efficiency is becoming increasingly important when it comes to wireless technologies.

The Future of the Wireless Technology
The Internet of Thing is increasingly becoming reality. Ever more machines, devices, objects and - last but not least - people are becomig interlinked.

Smarte Kameras Haben Alles Sicher im Blick
Smarte Kameras mit integrierter Intelligenz können Bilder autark verarbeiten und eigenständig Aktionen auslösen. In der Industrie werden sie zur Qualitätskontrolle oder zur Steuerung von Anlagen eingesetzt.

Ist KI schlauer als der Mensch?
Was in den 1950ern mit einer Konferenz der KI-Pioniere John McCarthy und Marvin Minsky begann, ist zu einer Schlüsseltechnologie geworden. Sie beeinflusst schon heute unser Leben – und wird es mit steigender Intelligenz der Maschinen in Zu