Putting Power First - Powering Space 2.0

With Paul Leys

From a technology perspective, we have come a long way since the first lunar missions. Space is being commercialised in ways the pioneers could have only imagined. There are now almost 10,000 satellites in orbit around earth. Tourism may be the next frontier.  

The amount of processing power in an average low earth orbit (LEO) satellite is no doubt far more than that available during the moon landings. Of course, satellites don’t have the same legions of brilliant minds on hand to oversee every action, but that’s because they no longer need them. Processors are more capable of handling complex operations in real time, and we’re now seeing AI and Machine Learning being deployed in satellites, too.  

The number of LEO satellites in operation is increasing, in most part to meet the demand for global communications. But there is also talk of using the hostile environment of space to host other types of technology, such as data centres. That may not be entirely science fiction. With 5G coverage now available using LEOs, the communication activity and bandwidth in the area between the earth’s surface and the fringe of the Van Allen radiation belt is increasing rapidly.

Warning

Warning

Invalid configuration found. Contact the administrator.

 

Feature Versal AI Core XQR Series Versal AI Edge XQR Series
AI Engine Tiles 400  34
DSP Engines 1,968 464
Programmable Logic LUTs 899,840 150,272
Programmable Logic Memory 191 Mb 86Mb
PCI Express 4 x Gen4x8 1x Gen4x8
Multi-rate Ethernet MAC 4 1
Application Processing Units Dual-core Arm® Cortex®-A72
Real-Time Processing Units Dual-core Arm Cortex-R5F 
Gigabit Transceivers Ethernet (x2), UART (x2), CAN-FD (x2), USB 2.0 (x1), SPI (x2), I2C (x2)
Processor Memory 256 KB On-Chip Memory with ECC  

 

Renesas

ISLVERSALDEMO2Z

VC1902 AMD Xilinx Space Grade Versal ACAP AI Core Demonstration Board.

ISLVERSALDEMO2Z
Warning

Warning

Invalid configuration found. Contact the administrator.

 

Aerospace & Aviation

Space 2.0 Overview

We use our vast knowledge and long experience of supporting traditional radiation-hardened components to come up with innovative, lower cost, reliable radiation tolerant components. We're ready to support your next Space 2.0 project.

Earth's radiation - space 2.0 components need to be radiation hardened

Technology

Power: designing solutions with power at the core

We provide you with the right insights and expertise when you need it most, so you can make the right decisions for your product, and your business.

Power - Power components lighting up on board