AVS Automotive Subnavigation Sensing

Display portlet menu

Driving the Future: The Transformative Journey of In-Vehicle Networks

An in-vehicle network (IVN) is an automotive data communications system used to interconnect electronic control units. The modern vehicle is a mobile digital communications platform. The vehicle’s IVN ensures reliable communication between the myriad electronic devices within it and the outside world.

As vehicle designs have evolved to include infotainment systems, vehicle-to-everything communication (V2X), and advanced driver assistance systems (ADAS), the volume of data that flows within the IVN has increased dramatically. ADAS systems use real-time uncompressed data and sensor fusion, combining data from multiple sensors to create an accurate view of what surrounds the car. The time-critical nature of these systems also requires fault tolerance – a failure of one aspect of the circuit should not impact the system’s overall function. It is clear that the traditional automotive networking architecture CAN or LIN, with its limited bandwidth, would not be able to keep up with these data volumes and would not offer sufficient fault tolerance to be useful. In this article, we outline the evolution of the IVN from the distributed topology seen in legacy designs through the centralised, domain-based topology seen in today’s cars to the zonal topology that will feature in future vehicles.

The evolution of IVN architectures

The earliest incarnation of an IVN was the Local Interconnect Network or LIN, a simple single-wire protocol where a master controller controls a group of slaves, each identified by an ID. Invented later, in the late 1980s by Bosch, the connected area network (CAN) bus IVN is a point-to-point system that wires all ECUs (nodes) to each other. Communication is packet based via a single twisted pair cable. The data rate capabilities are comparatively low; the system is asynchronous, hence unsuitable for time-critical operation. However, it does feature a unique non-destructive arbitration method for handling message collisions. Both systems feature today for non-time critical systems such as windows, lights, rain sensors, and door locks. Several alternative protocols, including “FlexRay”, MOST, and CAN FD (FD = flexible data rate), came to market to increase data rate capabilities.

Figure 1 shows the various IVN types and data rates.

Graph showing IVN types and respective data rates

However, the benefits of scalability and adaptability that Ethernet offered made it an enticing choice for designers. To successfully integrate Ethernet into the automotive environment, modifications are needed to reduce susceptibility to electromagnetic interference (EMI), add time sensitivity (TSN), and improve robustness and reliability. By exploiting the versatility of the original Ethernet design, a modified communications interface (Physical Layer), more resilient to the hostile automotive environment, is implemented.

The modified physical layer employs single unscreened twisted pair (UTP) cable, transformer coupling, and full duplex capability, with a range of 15m.

Ethernet is exceptionally versatile; ECU nodes can be added at will without reprogramming. Collisions are eliminated because the system is full duplex (data can be transmitted and received simultaneously). Traffic is optimised, and virtual sub-networks are created by adding intelligent switches. 

ECUs connected in a ring topology, as shown in Figure 2, offer a level of parallel redundancy suitable for time-critical safety systems. As communication is full duplex, communication can occur in the other direction if there is a break in the ring at any point.

Interconnected ECUs

Ready to get started on your next Automotive project?

With decades of experience in working with a plethora of clients across EMEA, our Automotive experts are on hand to support you every step of the way, or whenever you need us.

Design Hub

The Avnet Silica Design Hub is the one-stop destination for your design and engineering needs. Design Hub information and solutions improve your time to market and help solve time-in-market challenges. Browse the hundreds of proven reference designs.

Webinar: In-Vehicle Networking / Connectivity

Is your in-vehicle network architecture ready for the next level of autonomous driving? 
Get ready with our on-demand webinar series.