Machine Learning - Unlocking the Future

Traditional software comprises instructions that electronic systems follow to perform specified actions. Machine learning inverts that by employing algorithms that instead enable systems to learn as they go along.

AI/ML analyzes incoming data by looking for patterns. It makes predictions or categorizations based on the patterns it has detected, and then it tests its predictions. The predictive model that the AI/ML creates is continuously revised and optimized.

AI/ML is well-suited for applications with large data sets or steady streams of data. It is especially advantageous when this kind of data must be processed quickly if not in real time. Typically data is structured, deliberately formatted before submitted to computation. AI/ML can certainly use structured data,  but because it is capable of learning it is particularly adept at processing unstructured data.

Some of the applications AI/ML works well for include:

  • Analytics and data
  • Autonomous systems
  • Environmental monitoring

CONTACT OUR AI EXPERTS

Key Machine Learning Applications

Analytics & Data

AI/ML excels at rapidly detecting patterns in vast amounts of data, which can be impractical (and sometimes impossible) to do with traditional computational systems. Furthermore, because AI/ML learns, it is also adaptable, meaning that with more data it can improve its models or even revise them if something fundamental in the nature of the incoming data changes. Almost any application can benefit from AI/ML, but it is of particular value in applications that rely on sensor input, notably in autonomous and semi-autonomous systems. 

Data funnel as pat of data analytics

Autonomous and semi-autonomous systems (MM)

Display portlet menu

Autonomous and semi-autonomous systems

Autonomous and semi-autonomous systems are entirely dependent on steady flows of sensor data. While autonomous systems can be trained in advance, it is not possible for a programmer to anticipate every object or circumstance any given autonomous system might confront. The capability to learn is critical. It enables the autonomous system to adapt to unexpected stimuli – a new object, or unfamiliar behavior from recognized objects. It would not be practical to create products such as self-driving cars without AI/ML.

Autonomous system - robotic arm in factory

Environmental Monitoring

AI/ML is applicable to environmental monitoring for many of the same reasons that it is applicable to autonomous systems. Environmental monitoring is similarly a sensor-based application that produces a steady stream of data that needs to be analyzed in real time. The environments to be monitored can be anything from a clean room, where even tiny changes can be highly significant, to the outdoors, where conditions can be highly changeable. Either way, environmental monitoring benefits from AI/ML’s strengths.

Drones monitoring a coastal environment

Sound Analysis, Speech & Audio Processing

Analysis of sound is useful to identify the contexts related to audio signals, and to have an understanding of the environmental sounds. Speech & audio processing helps to analyze large amounts of natural language data to support the interactions between computers and human "natural" languages. This includes speech recognition, natural language understanding, and natural language generation.

 

  • Natural language processing (NLP) to generate human-computer interactions. NLP includes speech recognition, natural language understanding, and natural language generation.
  • Acoustic scene classification (ASC) to categorize audio signals into predetermined classes. ASC is similar to speech recognition, except that the target classes are different and more heterogeneous. ASC can identify the contexts (classes) related to the audio signals and can be used in different applications including security and surveillance for gunshot detection, or just to identify the environmental situation you are in (restaurant, metro station, city street, etc...).
  • Keyword Spotting (KWS) to detect predefined keywords in an audio stream. KWS is a technique to provide a hands-free interface for on voice-activated devices with limited resources and is used similar to AI voice assistants to detect wake words and keywords to trigger an action.
Sound waves - sound analysis

Featured Article

Machines that Learn: A Deep Dive into AI/ML Models and Algorithms

Artificial intelligence (AI) and machine learning (ML) can be used to pull insights out of huge volumes of information quickly and efficiently. AI/ML can also give machines the ability to process information similar to the way humans do. 

AI/ML can perform recognition and classification, predictive analytics, natural language understanding, and other tasks that are difficult or impossible to accomplish with traditional computing.

These capabilities lead to an impressive variety of use cases: voice recognition, autonomous driving, epidemiology, pharmaceutical design, software coding, financial trading, and more.

Learn More

Related articles

Close-up of automated machinery with robotic arms and circular glass components
Defect visual inspection using AI enables multiple emerging markets
By Michaël Uyttersprot   -   August 8, 2024
Technical article
Machine vision is enabling many existing and emerging markets. Security, manufacturing and industrial automation all use machine vision. Adding artificial intelligence (AI) inferencing at the sensor provides many benefits. Industrial automation combines ...
Read More
laptop with graphic overlay
How is AI changing the electronics industry?
By Philip Ling   -   May 22, 2024
Technical article
Artificial intelligence has the potential to influence every part of any company. As a trusted partner and leader in technology, Avnet has a responsibility to its customers and suppliers to consider the impact of AI from all angles.
Read More
tensors
Why AI and embedded design share the same DNA
By Philip Ling   -   May 22, 2024
Technical article
Intelligence comes in many forms. More of us are interacting with devices that appear to understand us. What and how they understand depends on the technology inside. How are embedded engineers implementing intelligence?
Read More
a-microchip-with-the-image-of-a-neural-network-on-the-top
Why AI must redefine processor architectures
By Philip Ling   -   May 22, 2024
Technical article
Artificial neural networks are complex, multi-layered and multi-dimensional arrays of interconnected numerical values. Executing the math behind those connections is at the heart of AI. This math is unlike any other in the digital domain.
Read More
Patients using continuous passive motion machines in a medical setting
Learn how AI and the latest CPM technologies optimize patient rehabilitation
By Avnet Staff   -   February 21, 2024
Technical article
Continuous passive motion (CPM) is now a critical part of patient rehabilitation. New technologies, including artificial intelligence, are helping medical OEMs take the next step to optimize patient therapy.
Read More
5G mast in a cityscape at night
What is the impact of using AI in 5G networks
By Avnet Staff   -   August 22, 2023
Technical article
AI is impacting the performance, security and maintenance of 5G networks. Network operators are racing to reap the benefits. AI promises to deliver returns on network investment and improve the end-customer experience along the way.
Read More
AI/ML DVI camera
Advancing quality control: The Evolution, Impact and Future of Defect Visual Inspection (DVI) in Manufacturing
By Michaël Uyttersprot   -   July 26, 2023
Technical article
In the complex realm of manufacturing, Defect Visual Inspection (DVI) has emerged as a critical process, evolving significantly over time.
Read More
A brain holograph over an MCU chip
Placing greater intelligence at the edge
December 15, 2022
Technical article
With the number of connected nodes that make up the Internet of Things (IoT) growing on a daily basis, it is universally accepted that the way in which machine learning (ML) inferencing is executed has to change.
Read More
Contact us

Submit your inquiry via the form below.

 
 

Tools

Design Hub

Browse and review over a thousand proven reference designs to accelerate your design process. Try our design tool and then export it to your CAD tool of choice.

Training & Events

Learning for better, faster projects builds

Connect with the Avnet Silica experts who will guide you to reach further with your projects with on-going seminars, workshops, trade shows and online training.

Customer asking question at seminar.

Market

Smart City

Smart City is an opportunity to reimagine our cities with the goal to change our quality of life and to supply clean water and sufficient energy for all citizens in an environmentally sustainable and equitable way. Let's make our cities smart.

Smart City - Connected City

Contact us

Have a question?

Int. Freecall - 00800 412 412 11 | Product or shop-related inquiries: OnlineSupportEU@avnet.com | Content-related questions: yourmessage@avnet.eu