Technologies, techniques, and trends in energy management
Several popular topologies have emerged in power electronics, each with specific practical applications. The buck converter topology, for example, is a DC-to-DC step-down converter, the boost topology is a DC-to-DC step-up converter, and the half-bridge is a DC-to-AC step-down converter. MOSFETs and IGBT components are both used in these topologies, although the MOSFET, with its low gate-drive power, fast switching speeds and high efficiency at low voltages tends to dominate in a wide range of power electronic applications.
The quest for increased efficiency in power conversion is driving demand for higher voltage devices, however, and this trend is stretching the conduction loss and switching time limits of the traditional silicon MOSFET. Power electronics designers are increasingly turning to wide bandgap materials, like Silicon Carbide (SiC), which has several advantages over silicon. The low switching losses and high operating frequencies of SiC MOSFETs enable them to achieve superior efficiencies, particularly in higher-power applications requiring high current, and where high temperatures require enhanced thermal conductivity. SiC MOSFETs are now available that can withstand voltage thresholds up to almost 10kV, compared with 900V for silicon, and SiC’s higher critical breakdown field means that a reduced thickness device can support a given voltage rating, leading to significant size reduction.
Developing an energy management system therefore needs a thorough understanding of a wide range of techniques and careful choice of component and semiconductor technology. With so many factors to consider and time-to-market pressure demanding accelerated decision making, how can you make sure that your energy management application is optimised for both cost and performance?
Avnet Silica is here to support you
As an industry-leading force in power electronics, Avnet Silica has the capabilities to help you select the best power technologies for your energy management solution, without exceeding your budget.
Whether the answer is to build or buy, module or discrete design, our experts are here to help your team weigh the options and specify the best power solution for your application. With a comprehensive portfolio of products from the world’s leading suppliers of power electronics, Avnet Silica has the inventory in place to support you, particularly when time to market is critical. When you work with us you have direct access to our relationships with these suppliers and the insights which will ensure you make the right decisions.
From system design to application engineering, and prototyping, Avnet Silica’s specialist power team provides the products, technical support, regulatory compliance advice and design services to help you develop and optimise your solution. It's an exciting time to be involved in the power industry, and Avnet Silica is here to support you every step of the way.
CONTACT OUR POWER EXPERTS
Featured Energy Management podcasts
We Talk IoT Podcast - Episode 57: Optimising Power Efficiency with IoT
With rising energy costs and a greater push toward sustainability, industries are increasingly turning to IoT solutions to optimise energy consumption and reduce waste. IoT is not only about smart devices but also about gathering data to make smarter decisions that drive both efficiency and sustainability.
We explore the impact of IoT on energy efficiency and sustainability with Andy Richardson, VP of business development at Salom Europe. And delve into how data collected through IoT-enabled power supplies can lead to significant CO2 emissions savings, equivalent to saving thousands of trees. Our discussion highlights the necessity of understanding power usage profiles for accurate emissions reporting and legislation compliance and the broader implications for businesses aiming to achieve net-zero emissions by 2030. Andy shares insight into Salom's strategies and how companies can leverage IoT to drive new business models and make informed decisions.
Episode 37: Unleashing the Power of Wind Energy
Hold on to your hats: In today’s episode, we discuss one of the fastest-growing renewable power sources: wind energy. Did you know that a single wind turbine has the potential to generate enough electricity to power 1,400 homes?
In this episode, we welcome Barry Thompson, CEO of Alpha 311.
We'll unpack how cutting-edge technologies and ingenious strategies are evolving in this sector, emphasizing the impact of IoT in enhancing turbine efficiency. Our discussion will also cover the ecological benefits of wind power and a forward-looking perspective on this form of renewable energy.
Featured Energy Management solutions