behind-the-datasheet-vision-systems

Display portlet menu

behind-the-datasheet-vision-systems

Display portlet menu

Behind the Datasheet: Vision systems

Philip Ling

Image sensors are highly integrated devices, often with multiple operating modes and configuration parameters. Far from being a drop-in device, they need to be carefully integrated into the hardware, and require strong support from the system’s embedded software.

As with all system-level components, there needs to be a robust and flexible interface between the hardware and the software. This typically means using a driver: a software component that acts as the counterpart to the hardware element. The driver provides the system’s software a way to access the features of the hardware component. As such, drivers are often specific to a particular component, at least at some level.

Generic drivers can be used, and these do provide a good starting point for developers, particularly if the hardware component uses industry-standard interfaces. Drivers are often — not always — developed and provided by the hardware component manufacturer. To compound the issue, drivers are also normally specific to the operating system being used (if any).

One of the reasons why Linux is now so popular is because it comes with a lot of drivers. The community is also very good at developing and sharing drivers. Periodically, stable drivers may be integrated into the latest Linux distribution. If a Linux driver exists for the hardware component, it can save the engineering team a lot of time and effort.

This isn’t always obvious to developers when they begin the process of selecting an image sensor for their embedded vision application.

In this interview, Avnet Technical Marketing Engineer Mario Bergeron explains what engineers need to think about both before and after selecting an image sensor.

關於作者

Philip Ling
Philip Ling

Philip Ling is a Technical Content Manager with Avnet. He holds a post-graduate diploma in Advanced ...

behind-the-datasheet-vision-systems

Display portlet menu

behind-the-datasheet-vision-systems

Display portlet menu
相關文章
Avnet_case_study_series_wear_tech_part_1
AI-powered wearable targets preventable deaths – Part 1
By Philip Ling   -   2024年4月5日
Proof of Concept. The first part in an Avnet Case Study Series
sensor image close up
Choosing the right image sensor for machine vision applications
By David Hustler   -   2023年1月6日
The core component in any machine vision system, the image sensor has a major influence on product performance—but there's no universal right fit. There are many aspects to consider, and every manufacturer's product is different.

behind-the-datasheet-vision-systems

Display portlet menu
相關活動

未找到相關活動