Connecting the future
From developing small cells to be mounted outdoors close to telecommunications equipment to meeting the new requirements of edge computing, Avnet is a part of the process of bringing you the solutions of the future.

Signaling the future of 5G
Avnet's solution is Zynq® UltraScale+™ RFSoCs which can integrate multi-gigasample RF data converters into an SoC architecture.
Optimizing the Potential of 5G
5G technology enables smart mobile and other types of devices to remain ‘ever-connected’, and empowers users to realize the benefits of eMBB, URLLC , and mMTC technology.
Going the distance with smart wristbands
To minimize the time needed to create new wearable products, Avnet solution team has built a platform based on the Nordic nRF51 BLE Wristband Reference solution.

Meeting 2nd wave 5G NR requirements
The Zynq RFSoC DFE incorporates a hardened DFE subsystem and enables more processing per channel, greater instantaneous bandwidth, more integration and is cost-effective for high volumes.

Smarter wristband solutions are now at hand
Handy in size yet brimming with useful features, Avnet's smarter wristband solution designed with low power demand is the ideal platform to build sought after wearables that propel their organizations into the marketplace.

Accelerating the implementation of 5G
To speed up the implementation of 5G applications, Avnet brings you 5G modules FM150 and FG150 from Fibocom. Designed to the M.2 form factor, and the LGA form factor, these modules can cater to different industrial requirements.

Enhancing the performance of 5G
The onset of 5G has led to new applications as well as new requirements. To increase the flexibility of the network, the radio access network (RAN) architecture is now split into the centralized unit (CU) and the distributed unit (DU).